Excel MPC5777C clock configurator

cancel
Showing results for 
Search instead for 
Did you mean: 

Excel MPC5777C clock configurator

No ratings

Excel MPC5777C clock configurator

This config tool simplifies PLL setting calculation and clock configuration for MPC5777C device.

Version 1.3 added option to select between 264/300 MHz MCU versions.

               

Follow these steps

               

Note: Macros have to be enabled!

               

1. Enter frequency of used XOSC and desired PLL0 and PLL1 output.

     - put values into cells B14, Q13 and Q20 of the "Clocks" sheet

     - check if it is Valid or Invalid

     - "PLLconfig" sheet shows possible PLLs configurations                

 

2. Configure System and AUX clock selectors and its Dividers

     - check calculated frequency of System/Peripheral clocks

     - if Invalid change source clock and Divider value to keep Max freq

               

3. Copy generated code by pressing "Copy Code" button

Labels (1)
Attachments
Version history
Last update:
‎09-11-2020 03:45 AM
Updated by: