Example MPC5777M PinToggleStationery S32DS_1.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5777M PinToggleStationery S32DS_1.0

Example MPC5777M PinToggleStationery S32DS_1.0

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* start both Z7 cores, interrupts initialization, blinking three LED by interrupts,

* initializes and display notice via UART terminal and then terminal ECHO.

* Each core serves one interrupt and one LED.

*

* The example configures the device for maximum performance by initialization of

* instruction/data cache and enabling of branch prediction for each core

* (startup.s files).

*

* ------------------------------------------------------------------------------

* Test HW:         MPC5777M-512DS, MPC57xx Motherboard

* MCU:             PPC5777MQMVA8 0N78H

* Terminal:        19200-8-no parity-1 stop bit-no flow control on LINFlexD_2

* Fsys:               600MHz

*

* Debugger:        Lauterbach Trace32

*                  PeMicro USB-ML-PPCNEXUS

* Target:          internal_FLASH (debug mode, release mode)

* EVB connection:  USER LED1 connected to P8.0, LED2 connected to P8.1

*                  LED3 connected to P8.2

*

********************************************************************************

ラベル(1)
添付
コメント

Thanks,

How do you compile the code? What compiler did you use?

Thanks

Phil

評価なし
バージョン履歴
最終更新日:
‎03-09-2016 08:08 AM
更新者: