Example MPC5777C-eQADC_Simple GHS714

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5777C-eQADC_Simple GHS714

Example MPC5777C-eQADC_Simple GHS714

********************************************************************************
* Detailed Description:
* Initializes eQADC module and cyclically converts chosen channel, displaying
* it into terminal window.
* User could connect EVB pot's wiper to pin header W (see below) to see valid
* conversion result.
* ------------------------------------------------------------------------------
* Test HW:         MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C
* MCU:             PPC5777CMM03 2N45H CTZZS1521A
* Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz
* Debugger:        Lauterbach Trace32
* Target:          internal_FLASH
* Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A
* EVB connection:  For ADC: J53-1 (EVB pot's wiper) --> PW7  - ANB16
*                                                       PW8  - ANB17
*                                                       PW9  - ANB18
*                                                       PW10 - ANB19
********************************************************************************

附件
无评分
版本历史
最后更新:
‎09-26-2017 01:16 AM
更新人: