Example MPC5775K-DMA_Transfer S32DS_1.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5775K-DMA_Transfer S32DS_1.0

Example MPC5775K-DMA_Transfer S32DS_1.0

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* setup clock for peripherals, setup access right for Masters and Peripherals

* on AIPS_0

*

* DMA transfers block of data from variable TransmitBuffer to the variable

* ReceiveBuffer. Both variables are placed in SRAM.

*

* ICache and DCache are both disabled in startup file using CACHE_ENABLE macro.

* You can change the value of the macro at the following path:

* project Properties/C/C++ General/Paths and Symbols/Symbols

* If you change the value to 1, ICahce and DCache will be enabled in startup.

*

*

* ------------------------------------------------------------------------------

* Test HW:         MPC5775K-356DS, MPC57xx Motherboard

* MCU:             PPC5775KMMY3A 0N38M

* Fsys:            PLL0 266MHz

*                    Z4 Core 133MHz

* Debugger:        Lauterbach Trace32

*                  PeMicro USB-ML-PPCNEXUS

* Target:          internal_FLASH (debug mode, release mode)

* EVB connection:  default

*

********************************************************************************

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎02-11-2016 05:01 AM
更新者: