Example MPC5748G SIUL External Interrupt SDK PA BETA290 S32DS.Power.2017.R1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5748G SIUL External Interrupt SDK PA BETA290 S32DS.Power.2017.R1

Example MPC5748G SIUL External Interrupt SDK PA BETA290 S32DS.Power.2017.R1

********************************************************************************
Detailed Description:

Example shows configuration of SIUL External interrupts using SDK driver.
EIRQ0 (PA3) and EIRQ11 (PE12) are configured for detecting rising edge. 
Those pins are connected to switches SW1 and SW2 on DEVKIT board.
EIRQ1 (PA6) is configured for detecting falling edge.
Within its interrupt routines a LEDs are toggled upon edge detecting.

See PinSetting component for pins configuration within "Routing" and 
"Functionals Properties" tabs.

To see falling edge on PA6 just connect pin (J2.1) to GND shortly.


* ------------------------------------------------------------------------------
* Test HW:         DEVKIT-MPC5748G
* MCU:             PPC5748GSMKU6 0N78S
* Target:          Debug_FLASH
* EVB connection: 
* Compiler:        S32DS.POWER.2017.R1 
* SDK release:     S32_SDK_S32PA_BETA_2.9.0
* Debugger:        S32DS, Lauterbach Trace32
********************************************************************************
Revision History:
Ver Date        Author       Description of Changes
0.1 Jun-13-2019 Petr Stancik Initial version
*******************************************************************************/
ラベル(1)
添付
コメント

thank you very much

評価なし
バージョン履歴
最終更新日:
‎09-10-2020 02:37 AM
更新者: