Example MPC5748G PIT ISR GHS614

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5748G PIT ISR GHS614

Example MPC5748G PIT ISR GHS614

********************************************************************************

* Detailed Description:

* Example configure DRUN mode with PLL running at 160MHz.

* It also contain basic PIT and INTC driver for interrupt demonstration.

* On PIT timer timeout the PIT is triggering an interrupt which is served in PIT interrupt

* service routine.

* ------------------------------------------------------------------------------

* Test HW:     X - PC5748G - MB (rev C)

* MCU:          PPC5748GMMN6A

* Maskset:    1N81M

* Fsys:          160 MHz

* Debugger:    Lauterbach Trace32

*              

* Target:         Internal_FLASH

*

********************************************************************************

标签 (1)
附件
无评分
版本历史
最后更新:
‎04-24-2015 02:52 AM
更新人: