Example MPC5744P eTimer CTU ADC synchronization GHS614

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5744P eTimer CTU ADC synchronization GHS614

Example MPC5744P eTimer CTU ADC synchronization GHS614

********************************************************************************

* Detailed Description:

*

*

* This example shows synchronization between eTimer, CTU and ADC modules.

* The eTimer0 module timer 2 is initialized to generate PWM signal, and rising edge

* of this signal is used to generate trigger signal for CTU module. The CTU module

* use one command list with 4 ADC_0 channels. Single conversion mode is used,

* so ADC0 ch0, ch1, ch2 and ch3 are sampled.

* ------------------------------------------------------------------------------

* Test HW:  MPC57xx

* Maskset:  1N65H

* Target :  internal_FLASH

* Fsys:     200 MHz PLL with 40 MHz crystal reference

*

* EVB connection:

*

* P8.1  - A[0]  .. GPIO output, used to see CTU-ADC ISR period

* P9.1     - B[7]  .. ADC0 AN[0] input

* P9.2     - B[8]  .. ADC0 AN[1] input

* P16.4 - I[3] .. CTU0 EXT TRG output

*

* see CTU0 EXT TRG output signal (toggle on each trigger) on P16.4 with respect of eTimer PWM signals.

*

********************************************************************************

ラベル(1)
添付
コメント

Hi Pat,

Feel free to create a new thread. So others can also join a discussion.

If your questions are related to any issues in my examples than feel free to write here.

Peter

評価なし
バージョン履歴
最終更新日:
‎04-14-2015 05:23 AM
更新者: