Example MPC5744P PinToggleStationery S32DS_1.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5744P PinToggleStationery S32DS_1.0

Example MPC5744P PinToggleStationery S32DS_1.0

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* initializes interrupts, blinking one LED by interrupt,

* initializes and display notice via UART terminal and then terminals ECHO.

*

*

* Test HW:        X-MPC5744PE257DC, MPC57xx motherboard

* MCU:              PPC5744PFMMM8 1N65H

* Terminal:        19200-8-no parity-1 stop bit-no flow control on LINFlexD_0

* Fsys:             200 MHz

* Debugger:      Lauterbach Trace32

*                       PeMicro USB-ML-PPCNEXUS

* Target:          internal_FLASH (debug mode, release mode)

* EVB connection:  User LED 1 connected to A0 (P8.0),

*

********************************************************************************

标签 (1)
附件
评论

Hi   b55689

I think that this code should be fixed "Uart.h".....for example like "sys\uart.h"....

Please check this code..

Thank you.

无评分
版本历史
最后更新:
‎01-05-2016 07:36 AM
更新人: