Example MPC5744P PinToggleStationery S32DS_1.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5744P PinToggleStationery S32DS_1.0

Example MPC5744P PinToggleStationery S32DS_1.0

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* initializes interrupts, blinking one LED by interrupt,

* initializes and display notice via UART terminal and then terminals ECHO.

*

*

* Test HW:        X-MPC5744PE257DC, MPC57xx motherboard

* MCU:              PPC5744PFMMM8 1N65H

* Terminal:        19200-8-no parity-1 stop bit-no flow control on LINFlexD_0

* Fsys:             200 MHz

* Debugger:      Lauterbach Trace32

*                       PeMicro USB-ML-PPCNEXUS

* Target:          internal_FLASH (debug mode, release mode)

* EVB connection:  User LED 1 connected to A0 (P8.0),

*

********************************************************************************

ラベル(1)
添付
コメント

Hi   b55689

I think that this code should be fixed "Uart.h".....for example like "sys\uart.h"....

Please check this code..

Thank you.

評価なし
バージョン履歴
最終更新日:
‎01-05-2016 07:36 AM
更新者: