Example MPC5676R-eQADC_PMC_chnl_conv+calib CW210

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5676R-eQADC_PMC_chnl_conv+calib CW210

Example MPC5676R-eQADC_PMC_chnl_conv+calib CW210

********************************************************************************
* Detailed Description:
* Initializes eQADC module, performs calibration and cyclically converts PMC
* internal channel as specified by macros CHOOSEN_PMC_ADC_CHNL,
* CHOOSEN_PMC_ADC_SCALE and CHOOSEN_PMC_ADC_COMMAND to check particular voltage
* level, displaying it into terminal window.
* No external connection required excluding terminal via eSCI.
* ------------------------------------------------------------------------------
* Test HW:         XPC567XKIT516 - MPC567xADAT516 Rev.D, MPC567XEVBFXMB Rev.C
* MCU:             PPC5676RDMVY1 3N23A
* Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A
* Fsys:            180MHz
* Debugger:        Lauterbach Trace32
*                  PeMicro USB-ML-PPCNEXUS
* Target:          RAM, internal_FLASH
* EVB connection:  default
********************************************************************************

附件
无评分
版本历史
最后更新:
‎10-12-2023 05:45 AM
更新人: