Example MPC5676R DSPI-ext_SPI_memory-S25FL129P CW210

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5676R DSPI-ext_SPI_memory-S25FL129P CW210

Example MPC5676R DSPI-ext_SPI_memory-S25FL129P CW210

********************************************************************************
* Detailed Description:
* The example uses serial flash memory S25FL129P (connected to DSPI_PCS1)
* that is connected to DSPI_B module (PCS1). No Dual or Quad I/O has been used.
* SW uses polling mechanism.
* The example at first read device ID, performs bulk erase of S25FL129P and then
* programs some sample data specified in main function. Check reading is then
* performed. During that some notices are displayed on the terminal window.
* ------------------------------------------------------------------------------
* Test HW:         XPC567XKIT516 - MPC567xADAT516 Rev.D, MPC567XEVBFXMB Rev.C
* MCU:             PPC5676RDMVY1 3N23A
* Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A
* Fsys:            180MHz
* Debugger:        Lauterbach Trace32
*                  PeMicro USB-ML-PPCNEXUS
* Target:          RAM, internal_FLASH
* EVB connection:  default
********************************************************************************

附件
无评分
版本历史
最后更新:
‎10-04-2017 05:23 AM
更新人: