Example MPC5675K TSENS Temperature calculation CW210

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5675K TSENS Temperature calculation CW210

Example MPC5675K TSENS Temperature calculation CW210

********************************************************************************
* Detailed Description:
* Application performs basic initialization, setup PLL to maximum allowed freq.,
* initializes and display notice via UART terminal. It calculates temperature
* using TSENS and printes it to the terminal window.
* ------------------------------------------------------------------------------
* Test HW:        MPC5675KEVB
* MCU:            PPC5675KFMMSJ in Lock-Step mode
* Fsys:           180/150 MHz CORE_CLK
* Debugger:       Lauterbach Trace32
*                 PeMicro USB-ML-PPCNEXUS
* Target:         RAM, internal_FLASH
* Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A
* EVB connection: default
*
********************************************************************************

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎09-20-2016 03:38 AM
更新者: