Example MPC5674F eQADC+eDMA Single_Scan CW210

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5674F eQADC+eDMA Single_Scan CW210

Example MPC5674F eQADC+eDMA Single_Scan CW210

********************************************************************************

* Detailed Description:

* Initializes eQADC module, converts specified command queue and displays

* results into terminal window when EOQ is reached. Used analog inputs ANA_0 and

* ANA_1 requires external connection to converted voltage (potentiometer) to

* see some valid numbers. For simplicity, ADC module is not calibrated.

* ------------------------------------------------------------------------------

* Test HW:         XPC567XKIT516 - MPC5674ADAT516 Rev.C, MPC567XEVBFXMB Rev.B

* MCU:             PPC5674FMVYA264

* Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A

* Fsys:            264/200/150/60 MHz

* Debugger:        Lauterbach Trace32

*                  PeMicro USB-ML-PPCNEXUS

* Target:          RAM, internal_FLASH

* EVB connection:  Potentiometers     --> ADC inputs

*                  USER_DEV_RV2(J4-7) --> ANA_0 (J18-3)

*                  USER_DEV_RV3(J4-8) --> ANA_1 (J18-4)               

*

********************************************************************************

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎06-18-2015 12:46 AM
更新者: