Example MPC5644A eQADC channel 146 conversion+calibration CW210

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5644A eQADC channel 146 conversion+calibration CW210

Example MPC5644A eQADC channel 146 conversion+calibration CW210

********************************************************************************

* Detailed Description:

* Initializes eQADC module, performs calibration and converts channel 146

* (voltage level of VDD) to check core voltage level and displays it into

* terminal window. No external connection required excluding terminal via eSCI.

*

* ------------------------------------------------------------------------------

* Test HW:        XPC564AKIT208S and XPC564AKIT324S

* MCU:            SPC5644AMMG1,0M14X and SPC5644AMVZ1,0M14X

* Fsys:           150/132/120/12 MHz

* Debugger:       Lauterbach Trace32

*                 PeMicro USB-ML-PPCNEXUS

* Target:         RAM, internal_FLASH

* Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A

* EVB connection: default

*

********************************************************************************

ラベル(1)
添付
コメント

What needs to be modified in this example to read and convert AN17, channel 17?  Just the following?

PUSH_TO_CFIFO0( CAL |
                EOQ |
                MESSAGE_TAG(RFIFO0) |
                CHANNEL(17) );

評価なし
バージョン履歴
最終更新日:
‎08-07-2014 04:55 AM
更新者: