Example MPC5604P ADC setting for scan mode on TRK board CW210

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5604P ADC setting for scan mode on TRK board CW210

Example MPC5604P ADC setting for scan mode on TRK board CW210

This simple example shows the ADC setting for the scan mode and usage of Trimmer on TRK-MPC5604P board.

Use Trimmer to dim the LED1.

 

Regards,

Petr

 

 

********************************************************************************

* Detailed Description:

*

* ADC testing and usage of Trimmer on TRK board

*

* ------------------------------------------------------------------------------

* Test HW:  TRK-MPC5604P

* Maskset:  0M36W

* Target :  internal_RAM

* Terminal: no

* Fsys:     64 MHz with 8 MHz XOSC reference

* EVB connection:

*

* Use Trimmer to dim the LED1

*

* NOTE! Be sure the ADC is powered, J21 5V jumper ON

*

********************************************************************************

标签 (1)
附件
评论

Hello PetrS,

Thank you for the quick response. The problem was as simple as powering the ADC - i.e. setting J21 jumper ON.

Do you know whether there are similar examples

1- for a simple FlexPWM ?

2- using the eTimers as Quadrature Decoders?

Thank you in advance.

无评分
版本历史
最后更新:
‎02-26-2014 05:30 AM
更新人: