********************************************************************************
* Detailed Description:
* Example dimmes LED1 according on board potentiometr. LED2 and LED3 demostrates
* ADC watchdog functionality. LED2 is turned on when signal level is below LOW
* threshold, LED3 is turned on when signal is above HIGH threshold.
* Example also displays coverted results to the terminal window.
* ------------------------------------------------------------------------------
* Test HW: XPC560B 100LQFP, XPC56XX EVB MOTHEBOARD Rev.C
* MCU: PPC5604BE MLL 1M27V
* Terminal: 19200-8-no parity-1 stop bit-no flow control on LINFLEX_0
* Fsys: 64/48 MHz
* Debugger: Lauterbach Trace32
* PeMicro USB-ML-PPCNEXUS
* Target: RAM, internal_FLASH
* EVB connection: - initialize PB[8] as ANS0: connect potentiometer to PB[8]
pin, remove J30 jumper and connect J30.2 with P2.9
- header J8 (LED_EN) fully fitted
********************************************************************************