Example MPC5566EVB PinToggleStationery CW210

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5566EVB PinToggleStationery CW210

Example MPC5566EVB PinToggleStationery CW210

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* initializes interrupts, blinking one LED by interrupt, second LED by software

* loop, initializes and display notice via UART terminal and then terminal ECHO.

* The example configures the device for maximum performance (OPTIMIZATIONS_ON).

* Its intention is to offer advanced startup code additional to CW stationery.

* ------------------------------------------------------------------------------

* Test HW:        MPC5566EVB

* MCU:            PPC5566MVR132

* Fsys:           144/132/112/80/12 MHz

* Debugger:       Lauterbach Trace32

*                 PeMicro USB-ML-PPCNEXUS

* Target:         RAM, internal_FLASH

* Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A

* EVB connection: TPU_PORT_37 -> USER_LED_8

*                 TPU_PORT_38 -> USER_LED_7 (to see blinking LEDs)   

*

********************************************************************************

标签 (1)
附件
无评分
版本历史
最后更新:
‎05-15-2015 01:35 AM
更新人: