FRDM-MXCW71: Hands On 2: Recognize NBU Incompatible Versions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-MXCW71: Hands On 2: Recognize NBU Incompatible Versions

FRDM-MXCW71: Hands On 2: Recognize NBU Incompatible Versions

MCXW71 is a three-core platform that integrates a Cortex-M33 application core (CM33), a dedicated Cortex-M3 radio core, and an isolated EdgeLock Secure Enclave. The radio core, also called as Narrow Band Unit (NBU) features a Bluetooth Low Energy (LE) unit with a dedicated flash. The memories integrated in the NBU consist of Bluetooth LE controller stack and radio drivers. On MCXW71, only boot ROM has access to the NBU flash. The ROM bootloader provides an in-system programming (ISP) utility that operates over a serial connection on the microcontroller units (MCUs)

The objective in this hands-on, is to learn how to recognize when the NBU firmware does not match with the SDK version.

Lab guide: FRDM_MCXW71_Incompatible_NBU_Firmware_Version

Incompatible NBU Firmware: mcxw71_nbu_ble_1_9_10_0.sb3

Labels (2)
Attachments
No ratings
Version history
Last update:
‎10-11-2024 09:21 AM
Updated by: