simple pwm with FlexPWM0 MCXA153

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

simple pwm with FlexPWM0 MCXA153

Jump to solution
791 Views
berndgrossmann
Contributor II

I try to get a 1kHz PWM Signal on Pin 3.1 (45) of FRDM-MCXA153 board.

Peripheral is set to FlexPWM0 B,0 Pin to 45 Output

berndgrossmann_5-1732527655231.png

 

FlexPWM0 settings are

berndgrossmann_6-1732527655240.png

 

berndgrossmann_7-1732527655246.png

 

I try to get a controlled pwm Signal on pin 3.1 with on/off an duty cycle control.

Can someone help me?

0 Kudos
Reply
1 Solution
758 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @berndgrossmann,
You can take as reference the pwm example of FRDM-MCXA153 SDK.

Pablo_Ramos_0-1732558596331.png

In order to have a better understanding about the example you can take a look to the readme file. In there you will find and overview, hardware requirements, board setting and how to prepare the demo.

Hope it helps you!

View solution in original post

0 Kudos
Reply
1 Reply
759 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @berndgrossmann,
You can take as reference the pwm example of FRDM-MCXA153 SDK.

Pablo_Ramos_0-1732558596331.png

In order to have a better understanding about the example you can take a look to the readme file. In there you will find and overview, hardware requirements, board setting and how to prepare the demo.

Hope it helps you!

0 Kudos
Reply