I am newbie with NXP board. I have a board MCXN947 and I read the specification of this board. It mentioned 3 Flash: 2MB with ECC, 64 Mbit fro QSPI flash and 512 Mbit Octal flash. So when deploy tflite model on this board, which flash memory I will flash into? I am concern about this problem because may be I can not deploy a "large" model. I am using MCUXpresso and examples from SDK + Code Hub.
I surprised about small flash memory of this board compared to MIMXRT1xxx boards.
 Harry_Zhang
		
			Harry_Zhang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @Harry_Zhang
2 MB is very small. If my model size is larger than 2 MB. I don't want to reduce model size. What I need to do ? Can I use other flashes or external storage to run model? Thanks.
 Harry_Zhang
		
			Harry_Zhang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Sorry, I have one more question.
Whether I can use 64 Mbit QSPI flash for running example from SDK. If I can, I will use larger model on 64 Mbit QSPI flash.
Could you sharing with me guide or tutorial to runing SDK examples with 64 Mbit QSPI flash in the case we can?
 Harry_Zhang
		
			Harry_Zhang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @nnxxpp
YES, you can use 64 Mbit QSPI flash for running example.
You can refer to the hello_world_qspi_xip.
BR
Harry