Unable to program MCXN236VNLT custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to program MCXN236VNLT custom board

Jump to solution
946 Views
sstcor
Contributor II

Designed a PCB based on the MCXN236VNLT and am trying to program the board using an MCU-Link debug probe, but I am getting the following error.

LinkFlash tool outputLinkFlash tool output

 

Labels (2)
0 Kudos
Reply
1 Solution
917 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sstcor 

 

Please review the ​FRDM-MCXN236 board schematic and verify your hardware design, particularly the ​SWD interface and ​power circuitry.

https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM-MCXN236  

 

BR

Alice

View solution in original post

0 Kudos
Reply
3 Replies
918 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sstcor 

 

Please review the ​FRDM-MCXN236 board schematic and verify your hardware design, particularly the ​SWD interface and ​power circuitry.

https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM-MCXN236  

 

BR

Alice

0 Kudos
Reply
898 Views
sstcor
Contributor II

Hi @Alice_Yang ,

After reviewing the schematic, I noticed VDD_SYS on the board is outputting ~3.2V and the datasheet says it should be between 1.71-1.98 V. It's floating in the schematic. Is it normal on 100 pin package?

I have connected the following pins to MCU-Link.

MCU-LinkNXP MCXN236
VTarget3.3V
GNDGND
SWDIOSWDIO
SWCLKSWCLK
RESETRESET

 

Multimeter readings: VDD_MCU = 3.3 V, VCore = 1 V

satinder1_0-1743522807741.png

satinder1_1-1743522824235.png

 

0 Kudos
Reply
876 Views
sstcor
Contributor II
Issue resolved. Missing a 2.2uF capacitor on VDD_SYS pin.
0 Kudos
Reply