Unable to Update MCU-Link Firmware on Windows 10 (FRDM-MCXN947)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to Update MCU-Link Firmware on Windows 10 (FRDM-MCXN947)

971 Views
IvonOramasPolo
Contributor I

I am experiencing difficulties updating the firmware of the MCU-Link probe included with the FRDM-MCXN947 board.

Here are the details of my setup:

Operating System: Windows 10

MCUXpresso IDE: v24.12 [Build 148] [2025-01-10]

Firmware version: CMSIS-DAP V3.128 (as shown in the “Safely Remove Hardware” icon: MCU-LINK FRDM_MCXN947 (r0E7) CMSIS-DAP V3.128)

USB drivers: already updated

Device Manager: the probe is listed only as VcomPort 

 I have read the MCU-Link installation article and followed all the suggested steps

Despite all these steps, the firmware does not update automatically, and the manual update fails as well. The MCU-Link probe is not being fully recognized by the IDE, which prevents firmware management.

I would appreciate your assistance in resolving this issue so that the probe is properly detected and updated

Labels (2)
0 Kudos
Reply
1 Reply

875 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @IvonOramasPolo 

If your issue still is not solved, please download and install the latest firmware from:
LinkServer for Microcontrollers - NXP

 

Note: The LinkServer installer includes firmware update utilities for MCU-Link and LPC-Link2. 
You can find MCU-Link under: 
C:\nxp\LinkServer_25.3.31\MCU-LINK_installer\scripts  
 
Please feel free to contact me if still have any issue or concern.

 

BR

Alice

0 Kudos
Reply