Hi,
Since there are now many families within the MCX series, I'd like some guidance to narrow down
A good match would be HS-usb, 4x4mm package still 0.5mm pitch. one I2S. a few gpio's, price <$1.0/pcs
thanks alice,
I also looked at the LFBGA64 parts which are also 5x5mm
• MCXC443VMP (only 16K ram, so might be too little for the stack)
• MCXC444VMP (32K, and also 256K flash meaning slightly higher prise point)
another alternative might be the 
• LPC5514JEV59 series (59BGA = 4x4mm), higher price probably due to more memory
Hello @dav1
I recommend two products to you.
One is the MCXC243VFT. It mostly meets all your requirements, except for the body size. Its size is 7mm*7mm. For details, please refer to: https://www.nxp.com/part/MCXC243VFT.
Another one is the MCXC244VFM. The only requirement it doesn't meet is the price. The budgetary price is $1.05 USD for 10,000 pieces, and its features all meet your requirements. For details, please refer to: https://www.nxp.com/part/MCXC244VFM.
Both of the two products support Full-speed USB, not HS-speed.
BR
Alice