SDK Custom board, missing runner.yaml

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDK Custom board, missing runner.yaml

265 次查看
Peter19
Contributor II

When building according to
https://mcuxpresso.nxp.com/mcuxsdk/latest/html/develop/sdk/custom_board_development.html

west build -b frdmmcxa346_custom examples/demo_apps/hello_world -DCUSTOM_BOARD_ROOT=<your custom board root(could be absolute path or relative path)>

No runner.yaml is produced in  build output.

It seems like custom boards is not fully implemented in mcux extension

Regards

/Peter

标签 (2)
0 项奖励
回复
2 回复数

216 次查看
Peter19
Contributor II

We are not using Zephyr.

Regards

/Peter

0 项奖励
回复

225 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Peter19,

The link you are referring to is for development of a custom board outside the SDK, not using Zephyr.

Please follow this webpage instead: Board Porting Guide — Zephyr Project Documentation.

As mentioned on that website: "you can usually start by copy/pasting its board directory and changing its contents for your hardware."

The best method to do a custom board implementation using Zephyr based on one of our MCUs is by downloading the zephyr repository using the MCUXpresso extension for VSCode, then going into <Zephyr repository>\zephyr\boards\nxp, identifying the board that implements the same SoC (as the Zephyr guide mentions), duplicating the board and changing the name to a custom name. Then doing all the changes to adjust the files inside this new board folder to the new name, as well as changing the board device tree to the specific hardware of your custom board.

After doing this, the MCUXpresso extension for VS Code will show the new board when importing an example from the Zephyr repository you selected. Once you import a project for your new custom board, building the project as usual will result in the build process creating the runners.yaml file, as well as the rest of the files created specifically for your custom board.

I hope this helps.

BR,
Edwin.

0 项奖励
回复