Running normal tflite on MCXN947 without NPU mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Running normal tflite on MCXN947 without NPU mode

跳至解决方案
860 次查看
nnxxpp
Contributor IV

I have a question about Running normal tflite on MCXN947 without NPU mode.

I saw that in the eiq examples from  SDK of MCXN947, all use NPU tflite with NPU mode. As mu understanding we can run normal tflite without NPU mode on MCXN947 only by changing resolvers. Is that right?

标签 (1)
0 项奖励
回复
1 解答
840 次查看
marek-trmac
NXP Employee
NXP Employee

Hi Nhanh Nao,

without NPU it should work too. NPU is recommended for better performance, with NPU it can be ~40-50 times faster.

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button

在原帖中查看解决方案

0 项奖励
回复
2 回复数
841 次查看
marek-trmac
NXP Employee
NXP Employee

Hi Nhanh Nao,

without NPU it should work too. NPU is recommended for better performance, with NPU it can be ~40-50 times faster.

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 项奖励
回复
834 次查看
nnxxpp
Contributor IV
Thank you.
0 项奖励
回复