RT600/700 GPIO Slew Rate Control

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT600/700 GPIO Slew Rate Control

1,258 次查看
aaronchin
Contributor II

Hi NXP,

In the RT600 and RT700 reference manual there is a GPIO setting to configure a GPIO's slew rate. This setting is either "disabled (default)" or "enabled." How is this setting tuning the internal driving circuit of the GPIO in its disabled and enabled state? 

434544897_2453569051697205_5100220487723441969_n.png

Best,

Aaron

标签 (1)
0 项奖励
回复
1 回复

1,229 次查看
marek-trmac
NXP Employee
NXP Employee

Hi Aaron,

as a part of MCUxpresso Config Tools, there is Pin tool available. The tool allows to generate code for pin routing and also for electrical pin configuration.

MCUxpresso Config Tools can be downloaded as standalone tool or they are also integrated into MCUxpresso IDE.

Hope this help

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 项奖励
回复