RT1064 EVK touch screen not working with NXP demo app

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1064 EVK touch screen not working with NXP demo app

ソリューションへジャンプ
778件の閲覧回数
kboon
Contributor I

Hi,

I use gui-guider to compile and run NXP printer demo app on RT1064 EVK board and I could get the LCD to display the main page.  However, when I touch the button on the screen, it does not transit to the next screen.  The same app works fine in simulation mode on my PC.  What could be wrong?

Regards,

 kboon

ラベル(1)
0 件の賞賛
返信
1 解決策
738件の閲覧回数
kboon
Contributor I

I managed to resolve the issue by changing the project setting to use DEMO_PANEL_RK043FN02H instead of the default DEMO_PANEL_RK043FN66HS.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
739件の閲覧回数
kboon
Contributor I

I managed to resolve the issue by changing the project setting to use DEMO_PANEL_RK043FN02H instead of the default DEMO_PANEL_RK043FN66HS.

0 件の賞賛
返信
713件の閲覧回数
Sam_Gao
NXP Employee
NXP Employee

Thanks for the update. It seems done.

0 件の賞賛
返信
743件の閲覧回数
Sam_Gao
NXP Employee
NXP Employee

Hi  @kboon 

Would you please help provide some details about this issue, such as hardware setting, SW version, which example are you using to me? thanks.

I am not sure if we provided the touch feature basd on RT1064EVK board in our offical release.

 

B.R,

Sam

0 件の賞賛
返信