Program of RT1061 can not run with flexspi nor flash but well in ram.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program of RT1061 can not run with flexspi nor flash but well in ram.

591 Views
lsjshengll
Contributor II
I'm a beginner working on driving a LED driver chip via I2C with the RT1061. It runs fine in ram debug mode (LED lights up), but when using flexspi_flash_nor_debug, the hardware initialization fails both in IAR simulation or flashing with jflash. I can read the flash contents, so the code is loaded. I've checked extensively but can't find the cause. Could you please help? Thanks.
I'm using flexspi1, with code partially transplanted from the hello world example. 

The keil program in the attachment zip. Thank you so much.
 
 
0 Kudos
Reply
1 Reply

559 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @lsjshengll ,

Thanks for your questions!

I noticed that you already have another identical thread, so we can keep synchronization in your other thread.

Thanks in advance!

Bests,
Gavin

0 Kudos
Reply