One MCLK for two SAI-Interfaces

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

One MCLK for two SAI-Interfaces

584 次查看
HelloWorld121
Contributor I

Hello,

I use i.MX8m mini and, and I want to operate two SAI-Interfaces at the same time.  

It is possible to use a single MCLK for two SAI-interfaces (e.g. SAI5 and SAI6)????

If yes, are there any Disadvantages ??

 

标签 (1)
0 项奖励
回复
1 回复

563 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

The transmitter and receiver can independently select between the bus clock and up to three audio master clocks to generate the bit clock. The \consideration is if you use a shared MCLK signal for your SAI ports, SAI5 or SAI6 should be configured in Synchronous mode between ports.

Best regards.

0 项奖励
回复