MQTT with TLS on MCXN947

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQTT with TLS on MCXN947

575件の閲覧回数
nxpsachve
Contributor I

Hi,

    Is it possible to have security(wolfssl or mbedtls) with MQTT on MCXN947. I'm using FRDM board and couldn't find any combination of mqtt with tls or ssl examples. Is there any way to integrate security with MQTT on MCXN947?

Regards,

Sach

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

530件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @nxpsachve 

Yes, currently, there is no related demo about combination of mqtt and tls.

BR

Harry

0 件の賞賛
返信

522件の閲覧回数
nxpsachve
Contributor I
Hi Harry,
Do you have any suggestions for achieving this on the MCXN947, such as using a particular repository or resource that can be adapted for the board?
Regards,
Sach
0 件の賞賛
返信

453件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @nxpsachve 

I suggest that you can 

start with mbedTLS + MQTT because:

Both are in the SDK

Easier integration path

Supported by many embedded projects.

BR

Harry

0 件の賞賛
返信