[MCXN947] Maximum frequency value of FlexPWM signal out

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MCXN947] Maximum frequency value of FlexPWM signal out

279 Views
billie
Contributor II

Hi,

I'm trying to test sample codes of SDK about FlexPWM block with pwm_cm33_core0  in MCX-N9XX-EVK board.

Here is a question about maximum frequency of FlexPWM signal output.

Can I set "APP_DEFAULT_PWM_FREQUENCY" as 1MHz ~ 7MHz ?

In my test complementary FlexPWM signal output is not good when I set "APP_DEFAULT_PWM_FREQUENCY" as 1MHz.  

Please let me know the maximum frequency of FlexPWM signal output if there is limitation.

 

Thank you.

Regards,

Billy

Labels (1)
0 Kudos
Reply
2 Replies

252 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @billie,

Could you help me test whether changing the pair operation to independent allows you to reach the desired frequencies?

Best Regards,
Pablo

0 Kudos
Reply

239 Views
billie
Contributor II

Hi,

 

I got correct FlexPWM output signals upto 7MHz like attached picture.

Thanks for your help. 

 

Regards,

billy

Tags (1)
0 Kudos
Reply