MCXN947 GPIO5 clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCXN947 GPIO5 clock

1,124 次查看
chrisgulick
Contributor III

Which clock is used for GPIO5. I see gpio0-4 but 5 is missing.
Which kCLOCK is used for GPIO5/PORT5. Thank you.

excerpt from fsl_clock.h

kCLOCK_Port0 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 13), /*!< Clock gate name: Port0. */

kCLOCK_Port1 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 14), /*!< Clock gate name: Port1. */

kCLOCK_Port2 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 15), /*!< Clock gate name: Port2. */

kCLOCK_Port3 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 16), /*!< Clock gate name: Port3. */

kCLOCK_Port4 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 17), /*!< Clock gate name: Port4. */

kCLOCK_Gpio0 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 19), /*!< Clock gate name: Gpio0. */

kCLOCK_Gpio1 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 20), /*!< Clock gate name: Gpio1. */

kCLOCK_Gpio2 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 21), /*!< Clock gate name: Gpio2. */

kCLOCK_Gpio3 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 22), /*!< Clock gate name: Gpio3. */

kCLOCK_Gpio4 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 23), /*!< Clock gate name: Gpio4. */

标签 (1)
0 项奖励
回复
3 回复数

1,077 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @chrisgulick 

According to MCXN947 Reference Manual.

HangZhang_1-1714985860418.png

slow_clk provides the bus clock for gpio5.

Its status is enabled by default.

Hope this will help you.

BR

Hang

0 项奖励
回复

1,056 次查看
chrisgulick
Contributor III

Thank you. I did notice the slow clock for gpio5 but did not know it was on by default. Good to know I will give it a try and toggle my gpio based on port5.

0 项奖励
回复

1,053 次查看
chrisgulick
Contributor III

I also discovered port 5.2 defaults to ALT1. It needs to be set to ALT0 for gpio use. But it is working now as gpio for me. The fun begins.

0 项奖励
回复