MCXN547VNLT GPIO current limit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCXN547VNLT GPIO current limit

816 次查看
seanwu
Contributor IV

Dear sir,

Does the MCXN547VNLT GPIO have a minimum current and a maximum current limit?

 

Thanks.

BR,

Sean Wu

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

758 次查看
seanwu
Contributor IV

Dear @Alice_Yang ,

Thanks for your reply.

And I have a question of What is the difference between the table and yours?

Thanks.

BR,

Sean Wu

seanwu_0-1730945598542.png

 

0 项奖励
回复

782 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @seanwu 

Please ignore my last reply. You are correct. As noted in point 9 of your screenshot:

If VIN is greater than VDD_Px_MIN (= VSS - 0.3 V) or is less than VDD_Px_MAX (= VDD_Px + 0.3 V), then there is no need to provide current-limiting resistors at the pads. No current limitation is required because, within this voltage range, the internal protection diodes can effectively protect the pins.

If this limit cannot be observed, need refer :

Alice_Yang_0-1730968535300.png

 

BR

Alice 

 

 

 

 

BR

Alice

0 项奖励
回复