MCXN547VNLT GPIO current limit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCXN547VNLT GPIO current limit

830 Views
seanwu
Contributor IV

Dear sir,

Does the MCXN547VNLT GPIO have a minimum current and a maximum current limit?

 

Thanks.

BR,

Sean Wu

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

772 Views
seanwu
Contributor IV

Dear @Alice_Yang ,

Thanks for your reply.

And I have a question of What is the difference between the table and yours?

Thanks.

BR,

Sean Wu

seanwu_0-1730945598542.png

 

0 Kudos
Reply

796 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @seanwu 

Please ignore my last reply. You are correct. As noted in point 9 of your screenshot:

If VIN is greater than VDD_Px_MIN (= VSS - 0.3 V) or is less than VDD_Px_MAX (= VDD_Px + 0.3 V), then there is no need to provide current-limiting resistors at the pads. No current limitation is required because, within this voltage range, the internal protection diodes can effectively protect the pins.

If this limit cannot be observed, need refer :

Alice_Yang_0-1730968535300.png

 

BR

Alice 

 

 

 

 

BR

Alice

0 Kudos
Reply