MCXN236/x4x SPI max speed when connet more than one slave SPI device.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCXN236/x4x SPI max speed when connet more than one slave SPI device.

1,478 次查看
seanwu
Contributor IV

Dear sir,

Now I want to use MCXN236 Flexcomm to be SPI feature, and use CS[n] to connect to 1~4 slave SPI devices. I want to know the max speed when connect more than one slave SPI devices. What the max speed is, when using one CS to connect one slave SPI device ,and what the max speed is, when using two CS to connect two slave SPI device...

Thanks.

BR,

Sean Wu.

Weikeng

0 项奖励
回复
3 回复数

1,441 次查看
seanwu
Contributor IV

Dear  @Harry_Zhang,

You mean that if I use LPSPI6 in OD mode to connect two slave SPI devices with two CSs, then the two devices speed are still 75MHz, right? 

Thanks. BR,

Sean Wu.

 

0 项奖励
回复

1,425 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @seanwu 

Yes, because even if two devices are connected, only one device is working at the same time. They can all work at maximum speed.

 

Hope this will help you.

BR

Hang

0 项奖励
回复

1,445 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @seanwu 

According to MCXN23x data sheet

4.6.2 LPSPI switching specifications.

Frequency of operation

In OD mode  

LPSPI0–LPSPI2     25MHz

LPSPI3–LPSPI5     50MHz

LPSPI6–LPSPI7     75MHz

In SD mode

LPSPI0–LPSPI2     21MHz

LPSPI3–LPSPI5     32MHz

LPSPI6–LPSPI7     50MHz

In MD mode

LPSPI0–LPSPI2     12.5MHz

LPSPI3–LPSPI5     25MHz

LPSPI6–LPSPI7     25MHz

Then theoretically, both slave devices also support the same high speed,  the speed could remain the same as when connecting one device.

Hope this will help you.

BR

Hang

0 项奖励
回复