Dear sir,
Now I want to use MCXN236 Flexcomm to be SPI feature, and use CS[n] to connect to 1~4 slave SPI devices. I want to know the max speed when connect more than one slave SPI devices. What the max speed is, when using one CS to connect one slave SPI device ,and what the max speed is, when using two CS to connect two slave SPI device...
Thanks.
BR,
Sean Wu.
Weikeng
Dear @HangZhang,
You mean that if I use LPSPI6 in OD mode to connect two slave SPI devices with two CSs, then the two devices speed are still 75MHz, right?
Thanks. BR,
Sean Wu.
Hi @seanwu
Yes, because even if two devices are connected, only one device is working at the same time. They can all work at maximum speed.
Hope this will help you.
BR
Hang
Hi @seanwu
According to MCXN23x data sheet
4.6.2 LPSPI switching specifications.
Frequency of operation
In OD mode
LPSPI0–LPSPI2 25MHz
LPSPI3–LPSPI5 50MHz
LPSPI6–LPSPI7 75MHz
In SD mode
LPSPI0–LPSPI2 21MHz
LPSPI3–LPSPI5 32MHz
LPSPI6–LPSPI7 50MHz
In MD mode
LPSPI0–LPSPI2 12.5MHz
LPSPI3–LPSPI5 25MHz
LPSPI6–LPSPI7 25MHz
Then theoretically, both slave devices also support the same high speed, the speed could remain the same as when connecting one device.
Hope this will help you.
BR
Hang