MCXE317MPA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCXE317MPA

325 Views
Neo1096
Contributor III

I saw on the official website that there is a document for the MCXE317MPA chip, which seems similar to the S32K312. Are there any differences between these two chips, or have they solved any bugs of the S32K312?

Labels (1)
0 Kudos
Reply
1 Reply

266 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @Neo1096 ,

Thanks for your post. They are very similar, but not exactly the same.

We proposes 2 portfolios of microcontrollers with similar hardware configuration: S32K31 automotive microcontrollers focus on automotive applications requiring Automotive-grade components and certification.

MCX E31 focuses on industrial applications with industrial mission profiles and certification.
While S32K31 also serves industrial applications. MCX E31 provides a complete and more coherent environment with the rest of MCX portfolio for industrial applications.

For details on the key differences between the S32K31 and MCX E31 microcontroller families, as well as information regarding software-related aspects, please refer to this application note.

S32K31x to MCX E31x Migration Guidelines

Hope it helps.

BRs,

Celeste

 

------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply