MCXC244VFM ISP pin to stay in rom boot?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCXC244VFM ISP pin to stay in rom boot?

ソリューションへジャンプ
573件の閲覧回数
dav1
Contributor V

there is no mentions in the datasheet for MCX C 244 which pin to use for ISP / rom-boot.

 

ラベル(2)
0 件の賞賛
返信
1 解決策
552件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @dav1,

Thanks for your post.  

For MCXC244, the pin for ISP/rom-boot is the NMI pin. Please refer to the capture in datasheet below:

Celeste_Liu_0-1739952031687.png

Hope it can help you.

BRs,

Celeste

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
553件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @dav1,

Thanks for your post.  

For MCXC244, the pin for ISP/rom-boot is the NMI pin. Please refer to the capture in datasheet below:

Celeste_Liu_0-1739952031687.png

Hope it can help you.

BRs,

Celeste

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信