[MCX-N9XX-EVK] LCD issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[MCX-N9XX-EVK] LCD issue

跳至解决方案
1,225 次查看
bryan_hong
Senior Contributor I

dear nxp

As you can see in the LCD screen capture below, the output appears abnormal.

According to the document 'lvgl_examples_readme.md' included in the SDK, the MCX-N9XX-EVK is supposed to support the LCD-PAR-S035. Kindly review this issue.

bryan_hong_0-1751422746399.png

and I use below SDK and project

bryan_hong_1-1751423012368.png

bryan_hong_2-1751423052634.png

Thanks,
Bryan

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,187 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @bryan_hong 

I tested the mcxn9xxevk_lvgl_guider ( SDK_2_16_000_MCX-N9XX-EVK), it can work.

 

Harry_Zhang_1-1751597639243.png

Harry_Zhang_2-1751597672365.png

You can test it.

And i also tested the 'mcxn9xxevk_lvgl_guider_bm_cm33_core0'.

It can not work.

I will report it  to our SDK team.

Thanks for your information.

BR

Harry

 

在原帖中查看解决方案

0 项奖励
回复
9 回复数
1,105 次查看
bryan_hong
Senior Contributor I

Hi Harry

Yes, LCD work!!!

If the test for is completed, Could you inform me via email ?

-- The test is to check whether 'mcxn9xxevk_lvgl_guider_bm_cm33_core0' works in SDK 24.12.00.

Thanks,
Bryan

0 项奖励
回复
1,140 次查看
bryan_hong
Senior Contributor I

dear Harry

Please let me know once the following action have been completed.

 

And i also tested the 'mcxn9xxevk_lvgl_guider_bm_cm33_core0'.

It can not work.

I will report it  to our SDK team.


Thanks,
Bryan

1,200 次查看
bryan_hong
Senior Contributor I

dear Harry

The same result is presented with 'mcxn9xxevk_lvgl_guider_bm_cm33_core0'. Please refer to the image and the link below. Additionally, 'frdmmcxn947_lvgl_demo_benchmark_bm_cm33_core0' also shows the same result. I'm currently testing while modifying 'fsl_st7796s.c'.

bryan_hong_0-1751521068326.png

 

It's strange that the example isn't working—are there any clues we should check to investigate further?


Thanks,
Bryan

0 项奖励
回复
1,188 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @bryan_hong 

I tested the mcxn9xxevk_lvgl_guider ( SDK_2_16_000_MCX-N9XX-EVK), it can work.

 

Harry_Zhang_1-1751597639243.png

Harry_Zhang_2-1751597672365.png

You can test it.

And i also tested the 'mcxn9xxevk_lvgl_guider_bm_cm33_core0'.

It can not work.

I will report it  to our SDK team.

Thanks for your information.

BR

Harry

 

0 项奖励
回复
1,171 次查看
bryan_hong
Senior Contributor I

dear 

I can not found `mcxn9xxevk_lvgl_guider` as below.

bryan_hong_0-1751848741974.png

and Your SDK version differ from me.

Could you guide to me how to install same SDK you use and how to get `mcxn9xxevk_lvgl_guider ` you use ?

Thanks,
Bryan

0 项奖励
回复
1,166 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @bryan_hong 

1. first, you need to download the 2.16 SDK.

Select Board | MCUXpresso SDK Builder

Harry_Zhang_0-1751857415170.png

2. And import the downloaded SDK.

Harry_Zhang_0-1751857882639.png

3. Then import the mcxn9xxevk_lvgl_guider demo.

BR

Harry

 

0 项奖励
回复
1,151 次查看
bryan_hong
Senior Contributor I

thanks for your quick comments

I have installed as below.

bryan_hong_0-1751861305861.png

But How to execute #3 

3. Then import the mcxn9xxevk_lvgl_guider demo.

Thanks,
Bryan

0 项奖励
回复
1,147 次查看
bryan_hong
Senior Contributor I

I have founded as below.

bryan_hong_0-1751861951864.png

 

0 项奖励
回复
1,212 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @bryan_hong 

May I ask if the demo of mcxn9xxevk_lvgl_guider can be displayed normally?

BR

Harry

0 项奖励
回复