MCX C wakeup by LPUART using 9600 with external 32.768KHz crystal?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCX C wakeup by LPUART using 9600 with external 32.768KHz crystal?

1,523 Views
frank-lin-Sunon
Contributor III

We plan to use mcxc142 in our project.
Before starting the project, we want to confirm that mcxc142 uses an external 32.768KHz crystal as the LPUART(9600,8,N,1) clock source, and when the data arrives, the LPUART can wake up the mcu and no data lost or data errors.

#mcxc

 

0 Kudos
Reply
5 Replies

1,496 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @frank-lin-Sunon 

Yes, you can refer to this picture.

HangZhang_0-1723021551391.png

RUN WAIT STOP VLPR VLPW VLPS LLS

In these low-power modes, it is possible to wake up without losing data.

Hope this will help you.

BR

Hang

1,482 Views
frank-lin-Sunon
Contributor III

Hi @Harry_Zhang ,

Yes, we understand that LPUART can run in the mode you mentioned without data lost/frame error.

But based on our past experience, 32.768KHz is not enough to run 9600 baud rate, unless the IC itself is specially designed for this. Usually if it is, it will be written in the file. 

For example in silicon lab efm32zg datasheet:

EFM32ZG.png

Or for Nuvoton M480:   https://www.wpgdadatong.com/blog/detail/40814

 

So we wanted to confirm if mcxc142 can actually do this.

0 Kudos
Reply

1,461 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @frank-lin-Sunon 

I'm sorry, for MCX C, 32.768KHz is not enough to run 9600 baud rate.

BR

Hang

0 Kudos
Reply

1,455 Views
frank-lin-Sunon
Contributor III

@Harry_Zhang 

We know that we can use the internal 8M frequency divider to 2M as the LPUART clock source.
But the internal low-frequency error reaches ±3%. Usually the minimum requirement that does not cause UART communication abnormalities is 5%, but since it shares 5% with the peer MCU, the single-sided error requirement is 2.5%. Is our understanding correct?
Does NXP have any special suggestions for saving power in UART communication of 9600?

0 Kudos
Reply

1,377 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @frank-lin-Sunon 

Yes, your understanding is correct.

Abort saving power in UART communication.

I think you can reduce the baud rate and enter low-power mode.

BR

Hang

0 Kudos
Reply