I'm using the development board LPCXpresso55S69 with a LPC55S69 and a SD-card slot. The SDK example works fine and can read and write from and to the card. In my own project, while trying to read with f_open(), it stalls in the call to the semaphore wait method. Card inserting detection works as expected and the initialisation is - to my eyes - done exactly as in the SDK example "sdcard_fatfs_cm33_core0_sdcard".
Here is the call-stack where it just stops and waits for the semaphore getting free.
OSA_SemaphoreWait() at fsl_os_abstraction_bm.c:795 0x724a
SDMMC_OSAEventWait() at fsl_sdmmc_osa.c:69 0x2b74
SDMMCHOST_TransferFunction() at fsl_sdmmc_host.c:275 0x8ee6
SDMMC_Goldle() at fsl_sdmmc_common.c:117 0x909e
SD_Goldle() at fsl_sd.c:345 0x92a
SD_ProbeBusVoltage() at fsl_sd.c:1,944 0x25a0
sdcard_init() at fsl_sd.c:2,020 0x26c6
SD_Cardlnit() at fsl_sd.c:2,107 0x2816
SD_Init() at fsl_sd.c:2,290 0x2afa
sd_disk_initialize() at fsl_sd_disk.c:145 0x3344
disk_initialize() at diskio.c:117 0x911c
mount_volume() at ff.c:3,430 0x44ec
f_open() at ff.c:3,740 0x4baa
Any hints where I could search for the problem or which further information I could provide?
Thanks in advance,
Alex
Further search revealed, that the interrupt SDIO_IRQHandler() does not fire. I use the standard SD_HostInit() to initialize the host, which subsequently calls SDIF_TransferCreateHandle() that should set up the interrupt. Still, there's something missing I can't locate in the (user-) code.
Hi @Alexander_42,
Is there anything else on your code that might disable interruptions? You mention that you call the same initialization function "SD_HostInit()", but do you also make sure to initialize all the pins, clocks and other hardware necessary for the SD card to function properly on your application?
BR,
Edwin.
Hi Edwin and thanks for your reply.
I compared the code flow between both projects, and everything looks identical. So, unless I did oversee something, the ports and timers should be set-up identical. The interrupt not coming in points to some set-up issue though, so I will double check, also with the HW monitors in MCUXpresso.
Best regards,
Alex