Full Speed USB [ FRDM-MCXA153] : usb device not detecting detach event

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Full Speed USB [ FRDM-MCXA153] : usb device not detecting detach event

6,784件の閲覧回数
Gurunath
Contributor II

Hi, i have tested the usb cdc(single port) vcom example (frdmmcxa153_dev_cdc_vcom_bm) where it echoes back the characters received from host. I tried using a flag for device detach event in USB_DeviceCallback() function defined in application main code. It looks like there is no interrupt triggered for  detach event.

I have enabled detach event by defining macro USB_DEVICE_CONFIG_DETACH_ENABLE with value 1, but main isr function USB_DeviceKhciIsrFunction(), inside USB0_IRQHandler() is not getting called.

in main(), am trying to send message with delay and this is supposed to stop and print a debug message as flag is changed if interrupt has triggered. Please find below the attcahed images for screenshots and let me know if i need to do some configuration.

 

 

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

6,639件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Gurunath 

I suggest you use the below two methods.

1> Please use the attached signal from below parameters to detect attach (1) or de-attach(0)

g_UsbDeviceHidGeneric.attach = 0U;

 

2> Enable P2_12 as VBUS detection, and check the "SESS_VLD" bit status in CONTROL register as below

Alice_Yang_0-1723695202084.png

 

BR

Alice

 

 

0 件の賞賛
返信

6,769件の閲覧回数
Gurunath
Contributor II
example is from frdm-mcxa153 sdk
0 件の賞賛
返信

6,656件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Gurunath 

Thanks for your patience.

The same on my side. I will check it with internal. Then reply you .ASAP. 

 

BR

Alice

 

0 件の賞賛
返信