FRDM-RW612 Error: Verification failed @ address 0x18000000

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-RW612 Error: Verification failed @ address 0x18000000

6,367 次查看
nguterresn
Contributor II

Hey!

I've been trying to make the FRDM RW612 work. I was able to flash for a couple of times, until I've connected the Adafruit TFT 2.8 LCD screen on top of the Arduino Header presented in the board, and, after that, I was able to flash a few more times until something went wrong and I couldn't anymore.

I've tried everything at this points:

- Downloaded MCUExpresso, created a default build for the board and tried to flash: failed.

- Downloaded the LinkServer, change from JLink probe to CMSIS, tried to flash: failed.

- Played around with JLink console: I can read and write onto specific addresses, but I can't flash.

I've tried different builds, NXP examples and Zephyr samples (Blinky): does't work.

Here's an example of error message from JLink:

 

 

 

J-Link>loadfile /Users/nunoguterres/Downloads/zephyr.elf 0x18000000
'loadfile': Performing implicit reset & halt of MCU.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 113ms
Downloading file [/Users/nunoguterres/Downloads/zephyr.elf]...
J-Link: Flash download: Bank 1 @ 0x18000000: 1 range affected (65536 bytes)
J-Link: Flash download: Total: 0.648s (Prepare: 0.165s, Compare: 0.150s, Erase: 0.004s, Program: 0.145s, Verify: 0.107s, Restore: 0.075s)
J-Link: Flash download: Program speed: 440 KB/s

****** Error: Verification failed @ address 0x18000000
Error while programming flash: Verify failed.

 

 

 

 

And here is the example of a connection to JLink:

 

 

 

 

JLinkExe -Device RW612 -speed 4000 -if swd
SEGGER J-Link Commander V8.10 (Compiled Sep 25 2024 14:15:06)
DLL version V8.10, compiled Sep 25 2024 14:14:53

Connecting to J-Link via USB...O.K.
Firmware: J-Link MCU-Link V1 compiled Sep 24 2024 10:57:33
Hardware version: V1.00
J-Link uptime (since boot): 0d 00h 22m 48s
S/N: 1066319194
USB speed mode: High speed (480 MBit/s)
VTref=3.300V


Type "connect" to establish a target connection, '?' for help
J-Link>connect
Device "RW612" selected.


Connecting to target via SWD
InitTarget() start
SWD selected. Executing JTAG -> SWD switching sequence.
DAP initialized successfully.
  DMAP_REG_ID: DM-AP IDCODE detected: 0x002A0000
  DHCSR: 0x05100000
InitTarget() end - Took 2.71ms
Found SW-DP with ID 0x6BA02477
DPIDR: 0x6BA02477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x84770001, ADDR: 0x00000000)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)
Feature set: Mainline
Cache: No cache
Found Cortex-M33 r0p4, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
Security extension: implemented
Secure debug: enabled
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105900D PID 000BBD21 DEVARCH 47702A04 DEVTYPE 00 Cortex-M33
[0][1]: E0001000 CID B105900D PID 000BBD21 DEVARCH 47701A02 DEVTYPE 00 DWT
[0][2]: E0002000 CID B105900D PID 000BBD21 DEVARCH 47701A03 DEVTYPE 00 FPB
[0][3]: E0000000 CID B105900D PID 000BBD21 DEVARCH 47701A01 DEVTYPE 43 ITM
[0][5]: E0041000 CID B105900D PID 002BBD21 DEVARCH 47724A13 DEVTYPE 13 ETM
[0][6]: E0042000 CID B105900D PID 000BBD21 DEVARCH 47701A14 DEVTYPE 14 CSS600-CTI
Memory zones:
  Zone: "Default" Description: Default access mode
Cortex-M33 identified.

 

 

 


I've noticed this behavior has happened twice (in two boards). I really want to believe this has nothing to do with the LCD, since it would place the responsibility of this not working onto NXP/Adafruit hands and faulty design.

Has anyone experienced something like this?

 

标签 (1)
标记 (5)
25 回复数

3,789 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi all,

 

For future reference, I solved this issue using the method showed in How to solve flashing problems in FRDM-RW612 (flash lock) - NXP Community.

 

I hope this helps.

Regards,

Daniel.

4,346 次查看
jmitchell
Contributor II

I ran into this same problem when working with FRDM-RW612 boards. I encountered this problem once and was able to reproduce it on another board. It seems that attempting to flash the 0x18000000-0x1FFFFFFF section using zephyr stops the board from being able to re-flashed.

Here are the steps I used to reproduce this problem:

  1. Start with a FRDM-RW612 board fresh out of the box.
  2. Build frdmrw612_hello_world example in MCUXpresso IDE v11.10.0.
  3. Flash frdmrw612_hello_world onto the board using JLink v7.98h triggered via MCUXpresso. Flash is successful.
  4. Run frdmrw612_hello_world a few times and see "hello world." message appear in the serial terminal.
  5. In a separate window, pull the latest changes from the Zephyr Project main branch and initialize west.
  6. Using west, build Zephyr example "samples/hello_world" for the "frdm_rw612" board configuration. 

 

west build -b frdm_rw612 "samples/hello_world"​

 

  • Using west, flash the FRDM RW612 board (adding verbosity flag for debug messages). This fails with the "Verification failed @ address 0x18000000" error reported above.

 

west -v flash​

 

  • Try reflashing board using the frdmrw612_hello_world in MCUXpresso. This now fails with "Verification failed @ address 0x08000000" error reported above.

 

Things I've tried to restore device to a usable state:

  1. Mass erase (this seems to no longer work)
  2. Flash using an external JLink debugger (this yields the same results as using the MCU Link)
  3. Running MCU-Link installer scripts to update firmware
  4. Power cycling with different jumper configurations
标记 (2)
0 项奖励
回复

4,261 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

I am having some dependency issues with the west flash command; I will try to solve them and test it.

Meanwhile, I tested using the J-Link command line to flash it, and the example is able to boot. Does this also happen on your side?

*** Booting Zephyr OS build v4.1.0-rc3-147-gfb4bb5d7688f ***
Hello World! frdm_rw612/rw612

Regards,

Daniel.

0 项奖励
回复

4,249 次查看
jmitchell
Contributor II

What commands did you use on the JLink command line? Essentially how Zephyr is trying to flash the board is by generating a JLink commander script file with the following contents (some path names removed).

 

Generated commander script file:

ExitOnError 1
r
LE
loadfile "<path_to_workspace>\build\zephyr\zephyr.bin" 0x18000000
r
g
writeDP 1 0
readDP 1
q

 

The command being run:

'C:\Program Files\SEGGER\JLink\JLink.exe' -nogui 1 -if swd -speed auto -device RW612 -CommanderScript '<the_commander_script_file>' -nogui 1

 

0 项奖励
回复

4,238 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

For the J-Link CLI I used:

loadbin hello_world\build\zephyr\zephyr.bin 0x08000000
0 项奖励
回复

4,233 次查看
jmitchell
Contributor II

Right, so the thing we're trying to troubleshoot here is loadbin to address "0x18000000" and how to recover from that.

0 项奖励
回复

4,223 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Even on address 0x18000000 I didn't find any issue.

Please find my log down below.

PS C:\zephyrproject\zephyr\samples\hello_world> west build -bfrdm_rw612 --pristine
-- west build: making build dir C:\zephyrproject\zephyr\samples\hello_world\build pristine
-- west build: generating a build system
Loading Zephyr default modules (Zephyr base).
-- Application: C:/zephyrproject/zephyr/samples/hello_world
-- CMake version: 3.28.1
-- Found Python3: C:/Users/Daniel/AppData/Local/Programs/Python/Python311/python.exe (found suitable version "3.11.9", minimum required is "3.10") found components: Interpreter
-- Cache files will be written to: C:/zephyrproject/zephyr/.cache
-- Zephyr version: 4.1.0-rc3 (C:/zephyrproject/zephyr)
-- Found west (found suitable version "1.3.0", minimum required is "0.14.0")
-- Board: frdm_rw612, qualifiers: rw612
-- ZEPHYR_TOOLCHAIN_VARIANT not set, trying to locate Zephyr SDK
-- Found host-tools: zephyr 0.17.0 (C:/Users/Daniel/zephyr-sdk-0.17.0)
-- Found toolchain: zephyr 0.17.0 (C:/Users/Daniel/zephyr-sdk-0.17.0)
-- Found Dtc: C:/Users/Daniel/.mcuxpressotools/dtc-msys2/tools/usr/bin/dtc.exe (found suitable version "1.6.1", minimum required is "1.4.6")
-- Found BOARD.dts: C:/zephyrproject/zephyr/boards/nxp/frdm_rw612/frdm_rw612.dts
-- Generated zephyr.dts: C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/zephyr.dts
-- Generated pickled edt: C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/edt.pickle
-- Generated devicetree_generated.h: C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/include/generated/zephyr/devicetree_generated.h
-- Including generated dts.cmake file: C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/dts.cmake
Parsing C:/zephyrproject/zephyr/Kconfig
Loaded configuration 'C:/zephyrproject/zephyr/boards/nxp/frdm_rw612/frdm_rw612_defconfig'
Merged configuration 'C:/zephyrproject/zephyr/samples/hello_world/prj.conf'
Configuration saved to 'C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/.config'
Kconfig header saved to 'C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/include/generated/zephyr/autoconf.h'
-- Found GnuLd: c:/users/Daniel/zephyr-sdk-0.17.0/arm-zephyr-eabi/arm-zephyr-eabi/bin/ld.bfd.exe (found version "2.38")
-- The C compiler identification is GNU 12.2.0
-- The CXX compiler identification is GNU 12.2.0
-- The ASM compiler identification is GNU
-- Found assembler: C:/Users/Daniel/zephyr-sdk-0.17.0/arm-zephyr-eabi/bin/arm-zephyr-eabi-gcc.exe
Load components for RW612:
driver_common component is included.
driver_reset component is included.
device_CMSIS component is included.
CMSIS_Include_core_cm component is included.
device_startup component is included.
driver_lpc_gpio component is included.
driver_pint component is included.
driver_inputmux component is included.
driver_inputmux_connections component is included.
driver_ostimer component is included.
driver_flexcomm component is included.
driver_flexcomm_usart component is included.
driver_cache_cache64 component is included.
component_osa_zephyr component is included from C:/zephyrproject/modules/hal/nxp/mcux/mcux-sdk/components/osa/set_component_osa.cmake.
-- Configuring done (14.4s)
-- Generating done (0.5s)
-- Build files have been written to: C:/zephyrproject/zephyr/samples/hello_world/build
-- west build: building application
[1/147] Generating include/generated/zephyr/version.h
-- Zephyr version: 4.1.0-rc3 (C:/zephyrproject/zephyr), build: v4.1.0-rc3-147-gfb4bb5d7688f
[147/147] Linking C executable zephyr\zephyr.elf
Memory region         Used Size  Region Size  %age Used
           FLASH:       27912 B        64 MB      0.04%
             RAM:        6952 B       960 KB      0.71%
            SMU1:        510 KB       510 KB    100.00%
            SMU2:        140 KB       140 KB    100.00%
        IDT_LIST:          0 GB        32 KB      0.00%
Generating files from C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/zephyr.elf for board: frdm_rw612
PS C:\zephyrproject\zephyr\samples\hello_world>
PS C:\zephyrproject\zephyr\samples\hello_world> west -v flash
-- west flash: rebuilding
cmake version 3.28.1 is OK; minimum version is 3.13.1
Running CMake: 'C:\Users\Daniel\.mcuxpressotools\cmake-3.28.1-windows-x86_64\bin\cmake.EXE' --build 'C:\zephyrproject\zephyr\samples\hello_world\build'
ninja: no work to do.
-- west flash: using runner jlink
-- runners.jlink: reset after flashing requested
runners.jlink: JLINKARM_GetDLLVersion()=79603
-- runners.jlink: JLink version: 7.96c
runners.jlink: JLink commander script:
ExitOnError 1
r
LE
loadfile "C:\zephyrproject\zephyr\samples\hello_world\build\zephyr\zephyr.bin" 0x18000000
r
g
writeDP 1 0
readDP 1
q
-- runners.jlink: Flashing file: C:\zephyrproject\zephyr\samples\hello_world\build\zephyr\zephyr.bin
runners.jlink: 'C:\Program Files\SEGGER\JLink\JLink.exe' -nogui 1 -if swd -speed auto -device RW612 -CommanderScript 'C:\Users\Daniel\AppData\Local\Temp\tmp4uj63qihjlink\runner.jlink' -nogui 1
SEGGER J-Link Commander V7.96c (Compiled Apr  2 2024 12:35:23)
DLL version V7.96c, compiled Apr  2 2024 12:34:28


J-Link Command File read successfully.
Processing script file...
J-Link>ExitOnError 1
J-Link Commander will now exit on Error
J-Link>r
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link MCU-Link V1 compiled Oct  9 2024 11:01:41
Hardware version: V1.00
J-Link uptime (since boot): 0d 00h 10m 38s
S/N: 1060061514
USB speed mode: High speed (480 MBit/s)
VTref=3.300V
Target connection not established yet but required for command.
Device "RW612" selected.


Connecting to target via SWD
InitTarget() start
SWD selected. Executing JTAG -> SWD switching sequence.
DAP initialized successfully.
  DMAP_REG_ID: DM-AP IDCODE detected: 0x002A0000
  DHCSR: 0xFFFFFFFF
ROM entered ISP command handling loop. Re-enable the debug access.
InitTarget() end - Took 22.1ms
Found SW-DP with ID 0x6BA02477
DPIDR: 0x6BA02477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x84770001)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)
Feature set: Mainline
Cache: No cache
Found Cortex-M33 r0p4, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
Security extension: implemented
Secure debug: enabled
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105900D PID 000BBD21 DEVARCH 47702A04 DEVTYPE 00 Cortex-M33
[0][1]: E0001000 CID B105900D PID 000BBD21 DEVARCH 47701A02 DEVTYPE 00 DWT
[0][2]: E0002000 CID B105900D PID 000BBD21 DEVARCH 47701A03 DEVTYPE 00 FPB
[0][3]: E0000000 CID B105900D PID 000BBD21 DEVARCH 47701A01 DEVTYPE 43 ITM
[0][5]: E0041000 CID B105900D PID 002BBD21 DEVARCH 47724A13 DEVTYPE 13 ETM
[0][6]: E0042000 CID B105900D PID 000BBD21 DEVARCH 47701A14 DEVTYPE 14 CSS600-CTI
Memory zones:
  Zone: "Default" Description: Default access mode
Cortex-M33 identified.
Reset delay: 0 ms
Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 134ms
J-Link>LE
J-Link>loadfile "C:\zephyrproject\zephyr\samples\hello_world\build\zephyr\zephyr.bin" 0x18000000
'loadfile': Performing implicit reset & halt of MCU.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 123ms
Downloading file [C:\zephyrproject\zephyr\samples\hello_world\build\zephyr\zephyr.bin]...
Comparing flash   [100%] Done.
Erasing flash     [100%] Done.
Programming flash [100%] Done.
Verifying flash   [100%] Done.
J-Link: Flash download: Bank 1 @ 0x18000000: 1 range affected (65536 bytes)
J-Link: Flash download: Total: 1.116s (Prepare: 0.280s, Compare: 0.106s, Erase: 0.268s, Program: 0.216s, Verify: 0.110s, Restore: 0.132s)
J-Link: Flash download: Program speed: 296 KB/s
O.K.
J-Link>r
Reset delay: 0 ms
Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
  MSPLIM cleared
ResetTarget() end - Took 155ms
J-Link>g
Memory map 'after startup completion point' is active
J-Link>writeDP 1 0
Writing DP register 1 = 0x00000000 (0 write repetitions needed)
J-Link>readDP 1
Reading DP register 1 = 0x00000040 (0 read repetitions needed)
J-Link>q

Script processing completed.

PS C:\zephyrproject\zephyr\samples\hello_world>

 

Regards,

Danie

0 项奖励
回复

4,217 次查看
jmitchell
Contributor II

Weird, I don't know what is so different about my setup...

How is your board connected to your computer? Are you using USB/MCULink or an external JLink debugger? Also which jumpers are set?

 

I am plugged into the MCULink port via USB-C with jumpers JP4 and JP9 set.

0 项奖励
回复

4,196 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Only JP4 and JP9 are connected. I am using MCU-Link debugger.

By any chance, did you flash an RD-RW612-BGA binary to the FRDM-RW612 before?

Regards,

Daniel.

0 项奖励
回复

4,183 次查看
jmitchell
Contributor II

I do not believe so although it is possible since I do have RD-RW612-BGA projects on my computer.

 

If that were to be what happened, how would I go about recovering the device to get it re-flashable?

0 项奖励
回复

4,108 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

I encountered with a similar problem when flashing an RD-RW612-BGA Zephyr example into the FRDM and then re-flashing a different FRDM-RW612 binary into the FRDM board.

****** Error: Verification failed @ address 0x18000000
Error while programming flash: Verify failed.

 

The board will no longer respond after this. Not even using MCUXpesso IDE.

I managed to bring up my board using MCUXpresso Secure Provisioning Tool

I set my board in ISP mode and flashed an example app (C:\nxp\MCUX_Provi_v9\bin\_internal\data\sample_data\targets\RW612\source_images\frdmrw612_gpio_led_output.s19). After this, I was able to re-flash my board with the correct FRDM Zephyr example.

 

I hope this helps.

Regards.

Daniel.

 

0 项奖励
回复

4,100 次查看
jmitchell
Contributor II
Thank you! I will try this and see if it works.

4,252 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

UPDATE:

I just solve the dependency issues. I am able to flash using west flash without problem. 

 

hello world.
hello world.
hello world.
hello world.
hello world.
hello world.
*** Booting Zephyr OS build v4.1.0-rc3-147-gfb4bb5d7688f ***
Hello World! frdm_rw612/rw612

 

 

Flash log:

 

C:\zephyrproject\zephyr\samples\hello_world>west flash
-- west flash: rebuilding
ninja: no work to do.
-- west flash: using runner jlink
-- runners.jlink: reset after flashing requested
-- runners.jlink: JLink version: 7.96c
-- runners.jlink: Flashing file: C:\zephyrproject\zephyr\samples\hello_world\build\zephyr\zephyr.bin

C:\zephyrproject\zephyr\samples\hello_world>

 

 

For those that can't use the west flash command, I did the following:

pip install -U -r scripts\requirements.txt

Regards,

Daniel.

0 项奖励
回复

4,322 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Let me check.

0 项奖励
回复

5,411 次查看
nguterresn
Contributor II

Here is a list of all the boot registers/fuses 

 

shadowregs -i jlink -f rw612 printregs                  
  #   Interface   Id           Description             
-------------------------------------------------------
  0   Jlink       1066319194   Segger J-Link MCU-Link  
Register Name:        LOCK_CFG0
Register value:       0x2000
Register raw value:   0x2000

Register Name:        LOCK_CFG1
Register value:       0x0000
Register raw value:   0x0000

Register Name:        LOCK_CFG2
Register value:       0x000B
Register raw value:   0x000B

Register Name:        BOOT_CFG0
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        BOOT_CFG1
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        BOOT_CFG2
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        BOOT_CFG3
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        BOOT_CFG4
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        BOOT_CFG5
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        BOOT_CFG6
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        SEC_BOOT_CFG0
Register value:       0x0000
Register raw value:   0x0000

Register Name:        SEC_BOOT_CFG1
Register value:       0x0000
Register raw value:   0x0000

Register Name:        SEC_BOOT_CFG2
Register value:       0x0000
Register raw value:   0x0000

Register Name:        SEC_BOOT_CFG3
Register value:       0x0000
Register raw value:   0x0000

Register Name:        SEC_BOOT_CFG4
Register value:       0x0000
Register raw value:   0x0000

Register Name:        SEC_BOOT_CFG5
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        SEC_BOOT_CFG6
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        SEC_BOOT_CFG7
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        SEC_BOOT_CFG8
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        DCFG_CC_SOCU_NS
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        DCFG_CC_SOCU
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        LIFE_CYCLE_STATE
Register value:       0x0303
Register raw value:   0x0303

Register Name:        CUST_SK_MK[31:0]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[63:32]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[95:64]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[127:96]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[159:128]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[191:160]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[223:192]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[255:224]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[287:256]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[319:288]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[351:320]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[383:352]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        RKTH
Register value:       0000000000000000000000000000000000000000000000000000000000000000
Register raw value:   0000000000000000000000000000000000000000000000000000000000000000
0 项奖励
回复

5,340 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

I haven't seen a similar problem before.

Are you able to execute a mass erase?

Regards,

Daniel.

0 项奖励
回复

5,318 次查看
nguterresn
Contributor II

Hi, yes.

In theory, yes. Mass erase works, at least the command doesn't fail.

However, it doesn't seem to do anything.

 

Any other idea? We have a few more boards but are a bit afraid to test it out due to the instability state of this board.

标记 (1)
0 项奖励
回复

5,226 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Are you able to execute a mass erase from MCUXpresso?

Regards,

Daniel.

0 项奖励
回复

5,128 次查看
nguterresn
Contributor II

Yes. The program finishes the mass erase process but doesn't change anything, I still can't flash.

0 项奖励
回复

5,424 次查看
nguterresn
Contributor II

Another update. 

I built a binary and skipped the validation (L2, the one causing the error). The board flashes BUT, it still doesn't run properly.

So, I downloaded (through Jlink save bbin command) the flashed program inside the rw612. It matches the one I tried to flash sniping the verification. So, my guess now is that the Bootloader (boot ROM) is pointing to the secure area (0x1800_0000) instead of pointing to the non-secure area (0x0800_0000). This guess gains traction with the fact the the default zephyr configuration has the following options:

 

CONFIG_ARM_MPU=y
CONFIG_HW_STACK_PROTECTION=y
CONFIG_TRUSTED_EXECUTION_SECURE=y

 

0 项奖励
回复