FRDM-MCXN947: Detection of Disconnection of USB1_HS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FRDM-MCXN947: Detection of Disconnection of USB1_HS

跳至解决方案
615 次查看
John_Adams
Contributor I

Hi,


I would like to ask, on the FRDM-MCXN947 board I am using USB1_HS with OTG USB, I am trying to detect the connection and disconnection of this USB. Connection detection works fine, so I use this function:

 

 

usb_device_notification_t USB_State(usb_device_struct_t *pDeviceHandle)
{
	usb_device_ehci_state_struct_t *ehciState;
	ehciState = (usb_device_ehci_state_struct_t *)(pDeviceHandle->controllerHandle);

	if (0U != (ehciState->registerBase->OTGSC & USBHS_OTGSC_BSV_MASK))
    {
		return kUSB_DeviceNotifyAttach;
    }
	return kUSB_DeviceNotifyDetach;
}

 

 

However, for some reason this USB OTG register does not detect the disconnection correctly. Is it possible to use some other register to detect the disconnection?

 

Thank you for any advise!

John Adams

标签 (1)
0 项奖励
回复
1 解答
596 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

Please refer to the following community post on how to enable the detach detection: What is the best way to detect attaching and detaching of an usb cable between RT1020 (device) and a...

It is referring an RT1020, but it is the same process for the MCXN947.

BR,
Edwin.

在原帖中查看解决方案

0 项奖励
回复
1 回复
597 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @John_Adams,

Please refer to the following community post on how to enable the detach detection: What is the best way to detect attaching and detaching of an usb cable between RT1020 (device) and a...

It is referring an RT1020, but it is the same process for the MCXN947.

BR,
Edwin.

0 项奖励
回复