Hello,
In my engineering school we give labs to a very large number of students using more than 100 FRDM-MCXN947 board.
1) Our students successfully compiled download and run there first programs (RGB led blink, switch etc) during the first lab.
2) During the second lab some of them can't connect anymore to the on-board cpu to download and debug (I suspect that they have updated the firmware, as explained hereunder).
Here are the snapshots when entering the debug mode :
3) I disconnect the student board and connect my fresh new board with success !
(Since our labs, are installed with MCUXpresso IDE v11.9.1, I tried with the latest MCUXpresso without success connecting there boards again.)
My board (working) :
4) From 3) I see a difference between the probe firmware versions :
I tried to reverse the firmware to V3.128 but can't find it on your website.
On NxP site, I only found MCU-LINK_installer_3.140 which allows me to reverse the board to V3_140 but the problem is still the same
Do you know where I can find MCU-LINK_installer_3.128 ?
Is is normal that upgrading the firmware cause such issue ?
Do you have other ideas ?
Thank you for your help !
Thierry
已解决! 转到解答。
Dear Alice_Yang,
I finally succeed to recover our boards access with MUC-LINK :
I clicked several time STP ERASE button, spamming simultaneously the SW1/Reset button of the FRDM-MCXN947 board (to reset the processor) !
Many thanks for your help !
(This worked with any version of MCU-LINK CMSIS-DAP which was finally not the point)
The subject is closed/resolved
Have a gret day
Thank you Alice.
Unfortunlatly, the first step failed : SPT Erase give me this error message :
Then I clic "Erase" :
Clicking on "Test connection" return :
Is there a way to reset the processor to attempts to open the debug port ?
Thank you for your help,
Regards,
Thierry
PS : the complete screen capture hereunder in case it may helps :
Thank you Alice for your answer.
1) Unfortunatly, reversing successfully (hereunder) the version to 3.122 didn't resolve the issue.
2) I still get this message when entering download mode :
(I recall you that my other boards are running correctly on the same computer/MCUxpresso version with CMSIS-DAP V3.128 but can't find it. Anyway, I am wondering if the CMSIS-DAP version is the real issue...)
FYI the led blinky application initially downloaded on these boards is still running on the processor.
What can I do ?
Thank you in advance for any help.
Hello @tgrandpi
2. Create a new workspace in MCUXpresso IDE.
3. Import a new simple demo.
4. Build and download the program for testing.
Dear Alice,
Thank you for your answer.
Unfortunatly, the first step : STP Erase failed :
When I "test connection", I get :
Can you tell me please a way to reset the processor as suggested by the error message ? Is it possible without specific external hardware ?
Thank you,
Thierry
Dear Alice_Yang,
I finally succeed to recover our boards access with MUC-LINK :
I clicked several time STP ERASE button, spamming simultaneously the SW1/Reset button of the FRDM-MCXN947 board (to reset the processor) !
Many thanks for your help !
(This worked with any version of MCU-LINK CMSIS-DAP which was finally not the point)
The subject is closed/resolved
Have a gret day