FRDM-MCXA156 – mcuboot_opensource SDK Example Not Working in MCUXpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-MCXA156 – mcuboot_opensource SDK Example Not Working in MCUXpresso

262 次查看
CEPL_Dev
Contributor III

Hi,

I am currently working with the FRDM-MCXA156 board for evaluation of one of

our projects and using the SDK examples in MCUXpresso IDE.
I have tested basic examples such as:

 

  • frdmmcxa156_blink_led

  • frdmmcxa156_lpuart_interrupt_transfer

 These examples worked as expected.

 

However, while testing the frdmmcxa156_mcuboot_opensource example from the

same SDK, I encountered the following log message on the terminal:

 

 

Screenshot 2025-08-14 145505.png

 

I have followed the tutorial from the official documentation here:

link

 

Could you please suggest what might be causing this issue?



 

 

 

Regards
Prasanth
标签 (2)
0 项奖励
回复
2 回复数

251 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @CEPL_Dev 

Thanks for your question.

Please use the two projects together: "mcuboot_opensource" and "ota_mcubot_basic".
 
For detailed steps, please refer to readme.md.

Alice_Yang_0-1755166872242.png

If still have issue, please show all your steps, I help you check.

Thank you.

 

BR

Alice

 

0 项奖励
回复

242 次查看
marek-trmac
NXP Employee
NXP Employee

Hi @CEPL_Dev ,

you can also use Secure Provisioning Tool, see step-by-step procedure described in the user guide: Generic workflows — MCUXpresso Secure Provisioning Tool 25.06

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 项奖励
回复