Do the MCXA153 drivers support I3C HDR-DDR mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do the MCXA153 drivers support I3C HDR-DDR mode?

481件の閲覧回数
ASM
Contributor I

Hi,

  In the example code I have, I can see that there is at least some code to support DDR, but it doesn't seem to work. Is it fully implemented, and if so, is there an example of how to use it?

  Thanks

0 件の賞賛
返信
1 返信

466件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @ASM,

As mentioned on the following community post: Solved: Re: Does RT685 support I3C HDR-DDR mode? - NXP Community

HDR-DDR mode has issues on both the RT and MCX A devices, so please use SDR instead.

BR,
Edwin.

0 件の賞賛
返信