Confusing state diagram in AN14145 - Flash Memory Swap Features on MCX N Series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Confusing state diagram in AN14145 - Flash Memory Swap Features on MCX N Series

ソリューションへジャンプ
1,990件の閲覧回数
laodzu
Contributor IV

Looking at AN14145 and Figure 2, I am somewhat confused about the error cases when the attempt to run the first "logical" image does not boot. I.e. the diagram gives this possible execution order:

 

Is there a second image file? Yes

Whether second image version is greater than first?  No

Start first image

Startup successful? No

Start second image

Startup successful?  Yes

Run first image

 

The last state should be "Run second image". The same problem exists on the symmetric case when the second image should be tested first and does not boot.

I know, it's kind of cosmetic, but its really confusing.  Would be good to fix this in the document.

Thanks in advance!

https://www.nxp.com/webapp/Download?colCode=AN14145

ラベル(2)
1 解決策
1,962件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Thank you for your feedback! 
I will inform this suggestion to the corresponding team so it is considered. 

Best regards,
Omar

元の投稿で解決策を見る

3 返答(返信)
629件の閲覧回数
laodzu
Contributor IV

Ah, I just looked at the latest available version of this document, and it is still the same, e.g. my suggestion was not included into the document 

As it takes time to post such suggestions, this limits my willingness to spend such time in the future. To be honest, I think this is sad and not a good way to encourage a community.

0 件の賞賛
返信
1,953件の閲覧回数
laodzu
Contributor IV

Hi Omar,

thanks for passing on my feedback to the right team.  I appreciate that!

Best wishes

 Detlev

0 件の賞賛
返信
1,963件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Thank you for your feedback! 
I will inform this suggestion to the corresponding team so it is considered. 

Best regards,
Omar