Applicability of normal and Reduced drive strength in MC912DG128ACPVE microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Applicability of normal and Reduced drive strength in MC912DG128ACPVE microcontroller

746件の閲覧回数
Kiran40
Contributor I

Hello,

Writing this to get confirmation on does the normal and reduced drive strength are applicable to  IIC config on the Port IB or is it just for pins configured as IO.  

Kiran40_2-1742377931212.png

 

 

Regards, 

Kiran 

0 件の賞賛
返信
1 返信

721件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

the data sheet states...

"These bits select reduced drive for the associated port pins. This
gives reduced power consumption and reduced RFI with a slight
increase in transition time (depending on loading). The reduced drive
function is independent of which function is being used on a particular
port."

 

Best regards,

Ladislav