The following steps will guide you through opening the hello_world application. The instructions for compiling and debugging the Cortex M33 core are covered in the instructions below.
Please use IAR Embedded Workbench for Arm version 9.50.1 or above.
Open the desired example application workspace. Most example application workspace files can be located using the following path:
<install_dir>/boards/<sdk_board_name>/<example_type>/<application_name>/iar
Note: In case of building errors, make sure that the correct board is selected, right-click in Project → Options → General Options → Target → Device. Select the NXP MCU you are using and is supported by the IAR version you have installed.
hello_world application is now running on the MCU.